0120-769-103 (フリーダイヤル)   |  jpesales@dwyeromega.com (Email) 

DATASHUTTLE or DATASHUTTLE EXPRESS - A device does not work when connected to the passthrough port of the DS-EXP or DS

CAUSE: Some devices are not able to work with the DATASHUTTLE or DATASHUTTLE Express between them and the parallel port. This is typically the case with bidirectional devices that do not use the ECP standard. Most printers do work.

SOLUTION: If the device is ECP, put the port in ECP mode. If the device is not ECP, put it on another parallel port. If there is no other parallel port you must disconnect the DATASHUTTLE to use it.




MMV | 6 |