フリーダイヤル 0120-769-103
Emailjpesales@dwyeromega.com

Calibration Data Management Software for use with CLB Precision Calibrator, Model OMEGASW-I
DISCONTINUED PRODUCT

OMEGASW-I

Calibration Data Management Software for use with CLB Precision Calibrator, Model OMEGASW-I   DISCONTINUED PRODUCT  | OMEGASW-I

スクロールダウンし、全ラインアップをご覧ください

商品説明

This Series is no longer available!

CALIBRATION
Calibration Test Procedures
Calibration test procedures have been prepared for temperature, pressure and electrical instruments. Specific range settings and other instrument details are entered to establish an optimal calibration point pattern.

Ambient Temperature Sample
Before each calibration test, an ambient temperature sample is recorded with the Pt100 probe to report calibration temperature conditions.

Tag Number Database
Serial number, area, hook-up and loop information can be entered or edited for each tag number. The serial number will be compared with the serial number recorded in the field. Any difference in serial numbers is reported.

Instrument Details
All instrument data entered to set up a procedure are stored in a database. Select tag number and press details to view or print instrument settings and procedure characteristics.

Pass/Fail Tolerance
A level expressed in a percentage of span or reading can be entered to assist technicians in the field. Findings exceeding pressure or temperature transmitter tolerances are displayed on the calibrator screen for verification.

Calibration Equipment
The system has an equipment database to comply with most types of process instruments. OMEGASW-I has been prepared for the CLB calibrator and future calibrator models.

Calibrator Shows Test Results
Test point results are reported for verification after a calibration test has been finished.

Short Cut for Test Procedure Setup
Do you have instruments with equal specifications? Test procedures made before may be used for new tag numbers to avoid full setup.

Message and Instructions
Message can be freely edited to be prompted in the field. Messages may be inserted in the test procedure to prompt before each calibration point. With pressure instruments, the calibrator display automatically shows the pressure to apply for each calibration point.

Calibration Strategy
Calibration points and sequences are selectable to check calibrations on specific points and on hysteresis. Technicians can select the type of routine from the calibrator keypad. Available routines are As Found and As Left.

LOGGER
Single Channel Datalogger
With the OMEGASW-I, a calibrator can be used as a single channel data logger. Temperature, pressure or electrical signals are recorded at preset intervals. Data is recorded on the PCMCIA card and can be printed. A 1 Mb PCMCIA card can contain as many as 9000 samples.

Datalogger Timers
Logger procedures are prepared with take sample timer settings. Timers are available to set the time between samples and to set the time between groups of samples.

Test Bench Applications
Test point sequences as composed in your procedure allow you to take recordings of output and input readings simultaneously. Inputs and outputs can be combined freely to adapt to your application. Very useful for engine performance tests and process monitoring.

REPORT
Editor
Your report has space for additional text. Before printing, you can edit personal report comments. These comments are saved under the appropriate tag number and can be re-edited each time you want to print a report.

WORK ORDER
Technician Work Orders
A work order is a selection of instrument tag numbers due for calibration. You can have one or more work orders. Work orders can be edited by adding or deleting tag numbers.

Work Orders Prepared for Each Loop
If calibration is performed loop by loop, OMEGASW-I offers a filter to show all instruments in a specific loop.

Work Order Notes
You can enter notes for each work order. Notes can contain specific work order instructions like safety warnings or information about the tools you need. Notes are printed together with the work order.

DOWNLOAD
Downloading Work Orders
A selection of prepared work orders are downloaded on the PCMCIA card for field calibrations or logging. Card access for downloading is made either by an integral PF card slot or by the calibrator card slot.

RESULTS
Graphs
Calibration of pressure or temperature transmitters can also be shown in a graph. You simply press the GRAPH key to show or print calibration graphs for both "As Found" or As Left findings. A zoom facility allows you to adapt the % error scale.

Reports
The OMEGASW-I allows you to report calibrations extensively. Simply select tag number, date and test routine. Press REPORT to print a full ISO 9000 document.

UPLOAD
Results Files

After calibration or logging, the PCMCIA card contains results in DBF formatted DOS files. These files are ready to be read by OMEGASW-I commercially available databases. As the files contain all results nicely arranged in a tabular format, you can print a simple document straightaway.

Uploading Result Files
Card access for uploading is made either by an integral computer card slot or by the calibrator card slot. The upload screen in OMEGASW-I allows you to move one or more files from the PCMCIA card into a directory on your PC hard disk.

TWO WAYS TO DO YOUR FIELD CALIBRATIONS

Level-1:
Calibrator built-in test procedures are used to record calibrations manually. Level-1 shows calibrator screens to enter and record tag number, serial number and name. Very suitable for service contracting companies who do not have test procedures prepared on OMEGASW-I.

Level-2:
Prepared test procedures composed in OMEGASW-I are used to record calibrations automatically. Simply select a tag number to start a test procedure from the keypad. The test procedure will proceed non-stop or will wait before each recording for your acceptance.

For complete product specifications see the Related Links section at the bottom of this page.

注文する (部品番号ビルダーより掲載以外の製品もご選択いただけます)(注文数を入力の上、"カートに追加"をクリックしてください)
部品番号/Desc.
注文数
商品説明
OMEGASW-I
お問い合せ下さい   
納期: 
 
 
Software for use with CLB Calibrator
注: Consists of compressed programs on two 3.5" disks. and includes operating manual in English, German and French, a 1 Mb PCMCIA SRAM type 2 card, and a RS-232 cable with COM port adaptor.
We noticed you are from the US. Visit your local site for regional offers and live support.